Manage security trusts
Trusts authorize connections between computers.
FactoryTalk Historian ME uses the following types of trusts:
To view trusts defined on the Historian ME module
- Click theConfigure Historiantab, and then clickTrust Management.TheTrust Managementpage appears.The page displays both the default and the user-defined trusts.TIP:If theIP AddressandNetMaskboxes are left blank in trust definitions, they appear as 0.0.0.0.
The FactoryTalk Historian ME server compares incoming connection credentials with every trust login record. Each setting in a trust configuration is compared to the corresponding credential setting. Every setting that is not blank in the trust configuration must exactly match the passed credentials. Otherwise, authorization is not granted. When authorization is refused for one trust, the FactoryTalk Historian ME server continues to search the other records until it has exhausted the possibilities.
Provide Feedback