Edit point discovery rule files

To edit a point discovery rule file
  1. In the
    FactoryTalk Historian ME Rule Editor
    window, click
    Rule File Management
    .
    The
    FactoryTalk Historian ME User Defined Rule File List
    dialog box appears.
  2. Select the rule file that you want to edit, and then click
    Open
    .
    The rule file appears in the
    FactoryTalk Historian ME Rule Editor
    window.
    The rules defined in the file appear in the table.
  3. Make your changes to the rule file:
    • To change the file description, type a new one in the
      Description
      box.
    • To add a rule, click
      New
      .
    • To edit a rule, select the rule, and then click
      Edit
      .
    • To remove a rule, select the rule, and then click
      Delete
      .
      In the message box that appears, click
      Yes
      .
  4. Click
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal