View the default point discovery rule file
By default, FactoryTalk Historian ME provides a point discovery rule file named
ADDefault.xml
. It contains search criteria with which you find tags for the point creation process.The path to the
ADDefault.xml
file is the following:<Program Files (x86)>\Rockwell Software\FactoryTalk Historian ME\ME Rule Editor\ADDefault.xml
You can open the file from the Rule Editor, or in an XML editor.
To view the default rule file in the Rule Editor
- Go toStart > All Programs > Rockwell Software > FactoryTalk Historian ME Rule Editor > Launch Rule Editor.The FactoryTalk Historian ME Rule Editor window appears.
- UnderFile Management, clickView XML file.The file is displayed in your web browser.
Provide Feedback