Define point attributes
Point attributes tell FactoryTalk Historian ME how and when the server should collect data from a particular data source. They contain the following information:
- The location of the data source.
- The frequency with which the server should get new values from the data source.
- The value that the server can ignore.
- The data that is valid.
In the Historian web client, the point attributes are presented in the following groups:
Provide Feedback