Snapshot value

The
Snapshot value
group contains the following point attributes:
Use this attribute
To
Value
View the current value of the tag, which is based on the tag type.
Timestamp
View the current time and date of the current tag value.
These attributes do not contain any data when you are creating a point.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal