General
The
General
group contains the following point attributes:Use this attribute | To |
|---|---|
Name | Name the point, following these rules:
|
Descriptor | Type a basic description of the point. The description will be displayed in client applications and user reports. |
Extended Description | Specify a relevant expression or a tag name. For details, see Configure Trigger Input and Output points. Use this attribute only with trigger input and output points. |
Instrument Tag | Provide a full path to the controller and the tag from which the data is coming. If you replace the controller with a different one that measures the same process value, it is usually best to continue using the same point. Edit the point as required so that it will collect the new data. Use the following format of the path: [<controllerprojectname>_1_<controllerslotnumber>][<controllertagname>] When a source tag receives events from the controller, the tag that you set in this attribute reads (or writes back) events from the controller. Note:
|
Source Tag | Type the trigger tag name. If you type a tag name, the source tag referenced must not be high-speed or have a scan rate of faster than 1 second. Otherwise, the module will generate an error and you will not be able to save the point. Use this attribute only with the Trigger Input or Output tags. |
Type | Set the data type of the point values. When you change the point type, the archive subsystem closes the current archive record, and starts a new one with the new type information in the header. For points collected automatically, use the point type that most closely matches the point type in the source system. Choose from the following:
|
Digital Set | Select the type of digital set for the point. Choose from the following:
|
Scan Type | Determine the scan type for the point. Choose from the following: |
Scan On | Identify active tags. The active tags are updated. If you want a point to be the active point, set this attribute to On and the point source to FHTME . |
Typical Value | Type a reasonable value for a point. For a numeric tag, it must be greater than or equal to the value of the Zero attribute, and lower than or equal to the sum of the Zero and Span attribute values.The typical value range is between 0 and 100. The typical value range for the points of type Digital is between 0 and 1. |
Point Source | Identify the interface to which the point belongs. When you configure an interface, you specify a point source for the interface. All the points that belong to the interface must use that point source code as the value for the Point Source attribute.The default point source is FTME . Other options include:
|
Scan Rate | Set the time in seconds, which tells FactoryTalk Historian ME how often to collect the data. For the Trigger Input and Output scan types, it is recommended that the scan rate is defined as two seconds or longer. For details, see Use scan classes. |
Span Value | Set the difference between the top and the bottom of the range. This attribute is required for all numeric data type points. For Float16 point types, the Span value is used with the
Zero value for scaling values in the archive. The Span property
must be a positive value. If the value for a Float16 point type is greater
than the top of the range, it is recorded in the archive as Over Range .For other point types, the Zero and Span values do not affect the
values recorded in the archive. The Span property is also used when
defining a FactoryTalk Historian ProcessBook trend with a vertical scale of the
database. This attribute is not used for non-numeric points. |
Zero Value | Type the lowest value possible. This attribute is required for all numeric data type points. It does not have to be the same as the instrument zero, but that is usually a logical choice. The zero value range is between 0 and 100. |
Provide Feedback