Search
FactoryTalk Historian Machine Edition Help
Manage points
In this section you will learn about the following:
Recommendations related to managing points
Add points using the Add Points Wizard page
Add points using the Add Individual Points page
Manage individual points using the Edit Points page
Define point attributes
Configure scan types
Configure Trigger Input and Output points
Manage shortcuts
Use scan classes
Recommendations related to managing points
Add points using the Add Points Wizard page
Add points using the Add Individual Points page
Manage individual points using the Edit Points page
Define point attributes
Configure scan types
Configure Trigger Input and Output points
Manage shortcuts
Use scan classes
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal