Manage shortcuts
Shortcuts are user-defined names for connections with controllers located in a local or remote chassis. A shortcut additionally contains the CIP path to a controller in a chassis.
You can use shortcuts to:
- Assign meaningful names to controller connections.
- Search for data points in the Add Points Wizard and on theAdd Individual Pointspage.
In FactoryTalk Historian ME, you can perform the following actions on shortcuts:
- TIP:All actions performed on shortcuts are logged. You can view the logged information underAdvanced>System Log.
Provide Feedback