Delete shortcuts
To delete a shortcut
- ClickManage Points, and then clickManage Shortcuts.
- In the table, click the shortcut that you want to delete, and then clickDelete.If you want to delete the shortcut, clickOK.Otherwise, clickCancel.TIP:If deleting the shortcut might result in a change in the functionality of time synchronization or data collection, you will be prompted for confirmation.
When deleting shortcuts, consider the following points:
- If you delete a shortcut used for time synchronization, the time will no longer be synchronized after you save your changes.
- If you delete a shortcut used for collecting data, the data will no longer be collected from this shortcut after you save your changes. However, the data will be collected from the controller used in this shortcut if data points were defined for the controller before the shortcut was created.
Provide Feedback