Back up and restore configuration files

It is recommended that you periodically back up the module configuration. You should also back up the configuration whenever changes are made to it. In case you need to reset the module, you will be able to restore the configuration after the module resets.
This table describes the backup configuration that can be restored on which Historian module series.
Backup configuration
Can be restored on
Series A
Series A, B, or C
Series B
Series B or C
Series C
Series C
TIP:
You must have administrator privileges to back up or restore the module's configuration files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal