View the backup status and perform backup
To view the backup status
- Click theConfigure Historiantab, and then clickBackup And Restore.TheBackup and Restorepage appears.
- UnderBackup Status, view the details of the most recent backup of the system configuration:
- The status of the backup.
- The date of the backup.
- The name of the backup file.
- The size of the backup file.The backup file contains configuration information for the following:
- Data collection.
- Data storage.
- Data transfer.
- Security.
- Data server.
- Point server.
- Web server.TIP:If any changes have been made to the system configuration since the last backup, it is recommended to perform another backup.
- ClickBackupto perform the system backup.
Provide Feedback