Upload the backup file to the module

To upload the backup file from the client computer to the module
  1. Click the
    Configure Historian
    tab, and then click
    Backup And Restore
    .
    The
    Backup and Restore
    page appears.
    Under
    Upload to Module
    , the details of the last upload are displayed:
    • The time the backup file was last uploaded to the module.
    • The name of the last uploaded backup file.
  2. Click
    Browse
    .
  3. Locate the file that you want to upload, and then click
    Open
    .
  4. Click
    Upload
    .
    TIP:
    • You can also upload the backup file downloaded from one FactoryTalk Historian ME Module to quickly configure another FactoryTalk Historian ME Module.
    • Please take the following into consideration:
      • You can only have one backup configuration file at a time on the FactoryTalk Historian ME Module.
        Only the last version of the backup configuration is stored.
      • The name of the backup file may not exceed 80 characters.
      • The backup file must contain the
        .tar.gz
        extension in its file name.
      • If you upload an older backup file, it will overwrite any newer backup file.
      • The backup file cannot contain a space in its name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal