Download the backup file to a client computer
To download the backup file to a client computer
- Click theConfigure Historiantab, and then clickBackup And Restore.TheBackup and Restorepage appears.UnderDownload to Client, the details of the last download are displayed:
- The time the backup configuration file was last downloaded to the client computer.
- The name of the last downloaded backup configuration file.The name is based on the date and time that the file was created.
- ClickDownload.The button is inactive if no backup of the module has occurred.IMPORTANT:Editing the xml files is not recommended.
After downloading the file from the module, you can use an XML parser to modify the configuration. However, you should not change the following files:
- datacollection/dconf.xml
- datastorage/dsconf.xml
- datatransfer/dtconf.xml
Provide Feedback