Configure CodeMeter settings

CodeMeter activation servers have the following additional options:
  • Run Network Server.
    Select this checkbox to open the CodeMeter port and enable CodeMeter activation servers to distribute licenses. Clear the checkbox to deactivate the servers and close the server ports to incoming and outgoing data.
  • Use CodeMeter First.
    Select this checkbox to use CodeMeter activations when running
    Rockwell Software®
    products on this computer before using Flexera activations of the same feature name. Clear the checkbox to use Flexera activations first.
  • Apply.
    Click this button to change the CodeMeter server settings and restart the server. This button is disabled if no setting changes are pending.
  • WebAdmin.
    Click this button to launch the internal, web-based CodeMeter server administration utility.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal