Deny access to a firm code

Configure
CodeMeter
options to deny access to all computers to all activations of a specific firm code, such as 102389 or 6000458.
  • Keep these considerations in mind when configuring
    CodeMeter
    options:
    • Only activations that are currently on the server can be configured.
    • Changing the access rules might require a refresh of the
      CodeMeter
      server.
    • To configure a computer to be a CodeMeter server, select the
      Run Network Server
      box on the
      Advanced > Configure CodeMeter
      page.
To deny access to all computers to all activations of a specific firm code:
  1. Open
    FactoryTalk Activation Manager
    on the server computer and click the
    Advanced
    tab.
  2. Click
    Configure
    CodeMeter
    .
  3. Click
    Web Admin
    to open the
    CodeMeter
    WebAdmin utility.
    Tip:
    In the
    CodeMeter
    WebAdmin utility, click the help CodeMeterHelpIcon icon for more information on settings and parameters.
  4. In the
    Mode
    box, select
    Advanced
    .
  5. In the
    Advanced Mode Configuration
    box, under
    Specific access rules
    , click
    Add new Firm Code
    to open the
    Add Firm Code
    box.
  6. Select the firm code to configure and click
    Add
    . The firm code is added under
    Specific access rules
    .
  7. For the default action, select
    Deny
    . All computers are denied access to use the specific Rockwell Automation software activations of the firm code. However, computers are automatically allowed access to localhost (the server computer).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal