Restrict access to
CodeMeter
activations on a server

Configure
CodeMeter
options to exclude a specific computer from accessing all
CodeMeter
activations.
  • Keep these considerations in mind when configuring
    CodeMeter
    options:
    • Only activations that are currently on the server can be configured.
    • Changing the access rules might require a refresh of the
      CodeMeter
      server.
    • To configure a computer to be a CodeMeter server, select the
      Run Network Server
      box on the
      Advanced > Configure CodeMeter
      page.
To restrict access to
CodeMeter
activations on a server:
  1. Open
    FactoryTalk Activation Manager
    on the server computer and click the
    Advanced
    tab.
  2. Click
    Configure
    CodeMeter
    .
  3. Click
    Web Admin
    to open the
    CodeMeter
    WebAdmin utility.
    Tip:
    In the
    CodeMeter
    WebAdmin utility, click the help CodeMeterHelpIcon icon for more information on settings and parameters.
  4. On the
    Configuration
    menu, click
    Server > License Access Permissions
    .
  5. In the
    Mode
    box, select
    Basic
    .
  6. In the
    Mode Configuration
    box, click
    Add
    . The
    CodeMeter
    WebAdmin utility adds
    localhost
    automatically.
  7. Enter computer names that are allowed to access the
    CodeMeter
    activations on this server computer. Computers that are not included in the Basic Mode Configuration client list are not allowed to access the
    CodeMeter
    activations.
    FactoryTalk Activation Manager
    does not display activations on the
    Find Available Activations
    page and they cannot be checked out.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal