Reserve activations for users or computers
Configure
CodeMeter
options to reserve activations for specific computers.- Keep these considerations in mind when configuringCodeMeteroptions:
- Only activations that are currently on the server can be configured.
- Changing the access rules might require a refresh of theCodeMeterserver.
- To configure a computer to be a CodeMeter server, select theRun Network Serverbox on theAdvanced > Configure CodeMeterpage.
Configure
CodeMeter
options to reserve activations for specific computers or users:- InFactoryTalk Activation Manager, click theAdvancedtab.
- ClickConfigure.CodeMeter
- ClickWeb Adminto open theCodeMeterWebAdmin utility.Tip:In theCodeMeterWebAdmin utility, click the help
icon for more information on settings and parameters.
- On theConfigurationmenu, clickServer > License Access Permissions.
- In theModebox, selectAdvanced.
- In theAdvanced Mode Configurationbox, underSpecific access rules, clickAdd new Firm Codeto open theAdd Firm Codebox.
- Select the firm code to configure and clickAdd. The firm code is added underSpecific access rules.
- Under the firm code, clickAdd New Product Codeto open theAdd Product Codebox.
- Select the product name for the activation to be included and clickAdd.
- ClickAdd new access ruleto open theAdd Rulebox.
- ForAction, select the opposite of the default action. For example, if the default action isDenyfor access not covered by the rule, selectAllowfor the rule action.
- In theHost,Subnet,User, orGroupbox, enter an identifier for the computer to be allowed to borrow an activation.
- In theHOSTbox, enter the computer name or IP address for which access should be allowed, or
- In theSubnetbox, enter the IP address for which access should be allowed, or
- In theUserbox, enter the user for whom access should be allowed. Use the following format:DomainName\UserName or PCName\UserName
- In theGroupbox, enter a Windows user group for whom access should be allowed. Use the following format:DomainName\GroupName
- In theReservedbox, enter the number of activations to be reserved for the specified host, subnet, user, or group. The number of reserved activations cannot be larger than the number of activations on the server.
Provide Feedback