ChX view
Use the
ChX
view to configure a channel on 1756-IF8 and 1756-IF16 non-isolated analog input devices operating in floating point mode (Data Format = Float) or configure an input channel on the 1756-IF4FXOF2F device.Use the
ChX
view to:- Select input type and range
- Enter scaling values
- Specify the digital filter time
- If supported, enter a sensor offset
Provide Feedback