Configure a channel on an analog input device

Create a channel-level configuration specific to your application.
To configure a channel on an analog input device
  1. On the tab for the device, expand
    Channels
    , and then select an individual channel.
  2. In the
    ChX
    view, customize the parameters as needed.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal