ChX view parameters

The
ChX
view includes these parameters:
TIP: The available parameters vary based on the device being configured.
Parameter
Description
Input Type
Specifies the input type. Available options are:
  • Current
  • Voltage
Input Range
Specifies the operating range of the selected channel.
Sensor Offset
Specifies an offset value that is added to the input during the calibration calculation to compensate for inaccuracies of the sensor.
Engineering Units
Specifies the name of the engineering unit.
High Signal
Specifies the high scaling value in signal units, volts or milliamps. You must set this input point within the device default signal range. This value is scaled to the
High Engineering
value.
High Engineering
Specifies the value in user engineering units to which
High Signal
should be scaled. All values sent to and from the device are in engineering units.
Low Signal
Specifies the low scaling value in signal units, volts or milliamps. You must set this input point within the device default signal range. This value is scaled to the
Low Engineering
value.
Low Engineering
Specifies the value in user engineering units to which
Low Signal
should be scaled. All values sent to/from the device are in engineering units.
Digital Filter
Specifies the time constant, in milliseconds, for a digital first order lag filter on the input. The digital filter smooths input data noise transients for the selected channel on the module. A value of 0 disables the filter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal