Configure an input channel

Create a channel-level configuration specific to your application.
To configure an input channel on a high-speed analog I/O device
  1. On the tab for the device, expand
    Input Channels
    , and then select an individual channel.
  2. In the
    ChX
    view, customize the parameters as needed.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal