StringInput object

The StringInput object represents the intrinsic numeric input object. It is not a creatable object. StringInput objects are accessible through an Elements collection.
The object-specific properties and methods for the StringInput object are merged with the Element object's properties and methods. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal