Accepted event
Occurs when the operation signatures are authenticated and accepted.
Syntax
object
_Accepted
(PerformerUser as String
, PerformerComment as String
, ApproverUser as String
, ApproverComment as String
)where
object
– is the name of a display element of one of the following types: Button, Numeric Input, or String Input.Provide Feedback