gfxMouseButtonConstants

Use the gfxMouseButton constants with the MouseDown and MouseUp events.
gfxMouseButtonPrimary
(1) – the mouse button used to select objects. For a right-handed configuration, this is the left mouse button
gfxMouseButtonMiddle
(4) – the middle mouse button
gfxMouseButtonSecondary
(2) – the mouse button that brings up context menus. For a right-handed configuration, this is the right mouse button
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal