Recipe object
The Recipe object is an object the represents the intrinsic Recipe object. It is not a creatable object. Recipe objects are accessible through an Elements collection.
The object-specific properties and methods for the Recipe object are merged with the Element object's properties and methods. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback