Value property (Recipe object)

Returns or sets the recipe name that is displayed in the field. This is the default property of the Recipe object. Read/write. String.
Setting the value does not move the focus to the field.
Syntax
Recipe
.
Value
[ =
string
]
where
Recipe
– is the name of a Recipe object or an expression that evaluates to a Recipe object.
string
– is a string value that specifies the name of the recipe.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal