NumericInput object
The NumericInput object represents the intrinsic numeric input object. It is not a creatable object. NumericInput objects are accessible through an Elements collection.
The object-specific properties and methods for the NumericInput object are merged with the Element object's properties and methods. This extended object is what you see when you directly access the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback