Context menu of a trend chart
While running a trend chart, the context menu gives you access to snapshots that you can overlay on the display.
Use the context menu to:
- Align left– Aligns the selected overlay on the left edge of the runtime chart.
- Relocate– Relocates the selected overlay by dragging it on the runtime chart. To anchor the relocated overlay, click the chart. The point where you click becomes the starting location of the data held in the snapshot. Relocating an overlay changes its offset percentage.
- Show/hide– Overlays the selected snapshot over the current trend data or hides the selected snapshot.TIP:Use theRuntimetab to specify the options available from the context menu at runtime.
Provide Feedback