Anchor an overlay on a trend chart
Overlay a snapshot on a trend and anchor it by position, or time.
To anchor an overlay on a trend chart:
- Open the trend chart properties and then click theOverlaystab.If a snapshot is not already added to the trend, clickAdd, and select a snapshot name. ClickOK.
- Click theAnchorrow to toggle between thePositionandTimesettings.If you selectPosition, specify anOffsetpercentage. To anchor the overlay at the left edge of the runtime chart, set the offset percentage to 0.If you selectTime, double-click theStartrow to specify a starting time.
- Close the chart properties and run the trend chart control.
Provide Feedback