Use macros

A macro is a list of commands or command symbols stored in a text file. To run a macro you use its name just as you would a command. For example, you can type the name of the macro in the command line and then press Enter. The commands in the macro will be executed in the order in which they are listed.
IMPORTANT:
Prior to running the AppStart command to launch any external program, please verify and ensure the external program is safe and trusted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal