Parameters in macros
Macros can accept optional parameters. To specify an optional parameter in a macro, place a percent (
%
) sign followed by a parameter number after the command that will use the parameter. To indicate a percent in a macro, you need to insert two percent signs (%%
) because a single percent indicates a parameter.The single quotation mark (
If a macro name has spaces in it, enclose the name in double quotes, for example,'
) is a special character in FactoryTalk View
and cannot be used in nested macros. Instead, use the double quotation mark ("). "New Macro"
parameter.Type macro parameters after the macro name.
Provide Feedback