Example: Macro with two parameters

A macro named
OView
consisting of the three commands:
Display overview
Display %1 /q1
Set valve23 %2
does the following when the
OView
macro is run on the
FactoryTalk View SE
Client:
  • displays a graphic called
    overview
  • overlaps it in the upper right quadrant with the graphic Detail (parameter 1)
  • sets the data item
    valve23
    to Open (parameter 2)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal