Nested macros

A macro is used like a command and you can place one macro within another. This is called nesting.
Macros can be nested eight levels deep.
The single quotation mark (
'
) is a special character in
FactoryTalk View
and cannot be used in nested macros. Instead, use the double quotation mark (").
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal