Edit an SE client

Use the
FactoryTalk View SE
Client Wizard to edit an existing client configuration file. At any point you can click another tab to edit details in that page.
To edit an SE client file:
  1. On the home page, click
    Edit a client file
    .
  2. On the
    Select client file
    page, do one of the following:
    • Select a file name from the list of recent client files.
    • Click the browse button to select a file name and then click
      Edit
      .
    • Type the full path name and then click
      Edit
      .
  3. On the
    Startup components
    page, edit the settings if needed.
  4. To edit the following advanced settings, click
    Advanced
    .
    • Client window properties
    • Security and debugging
    • Other options such as navigation tracking, on-screen keyboard and so on.
  5. To finish the configuration, click
    Save
    or
    Run
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal