Advance settings - Security and debugging
The following table shows options in the page.
Option | Description |
---|---|
Enable auto logout | Select this check box to turn on the automatic logout feature. When auto logout is enabled, the current user will be automatically logged out after the specified inactivity period. If a Logout macro is specified, it will be run when automatic logoff occurs.The login of a new user will trigger the restart of the SE Client and the initial display will be loaded. If the startup macro is configured to open a specific display, that display will be loaded instead. In the Logout macro, you can configure a .Login command and a Display command to log in with a new user and open a specific display upon the logout of the previous user |
Inactivity period | The inactivity period is the number of minutes of mouse or keyboard inactivity, after which the client will automatically log out the current user. The number can be from 1 to 99. |
Open FactoryTalk View SE Client as view-only | Select this check box if the FactoryTalk View SE Client is to be opened as a view-only client.When a FactoryTalk View SE Client is opened in view-only mode, the user can only perform read operation (rather than read/write). This means that the followings are disabled:
Commands processed on the client are enabled, except Download , DownloadAll , RecipeProDownload , and RecipeProUpload .You can use the Desktop Lock tool to prevent users from restarting the system or switching to other applications from an SE Client window. |
Disable switch to other applications | Select this to prevent the user from using Windows hot keys to switch to another application from the client window. When this option is selected the user cannot set focus to other windows or the Windows desktop. |
Allow display code debugging | Select this check box to give the user access to the VBA Code editor. This allows the user to make changes to the Display Code associated with a graphic display. Tip: If code debugging is enabled, the user can open the VBA Code editor by pressing Alt + V. |
Provide Feedback