Create an SE client
Use the
FactoryTalk View SE
Client Wizard to create a client configuration. At any point you can click another tab to return to edit details on that page.To create an SE client:
- On the home page, clickCreate a client file.
- On theFile name and locationpage, type the name for the configuration file and specify where it will be stored, and then clickContinue.
- On theStartup componentspage, specify the settings of the application that the client will connect to.
- To set up the following advanced settings, clickAdvanced.
- Client window properties
- Security and debugging
- Other options such as navigation tracking, on-screen keyboard and so on.
- To finish the configuration, clickSaveorRun.
Provide Feedback