Multi-monitor deployment
FactoryTalk View SE
supports the automatic and dynamic management of multi-monitor deployment for HMI application displays. Multi-monitor provides you with more screens to view more information about process operations from a single workstation.FactoryTalk View SE
multi-monitor deployment offers the following advantages:- The monitor configuration is defined per client and can be unique per operator station.
- A client configuration can support an individual configuration of up to six monitors per HMI client.
- HMI displays can be displayed on the specific pre-configured monitors or dynamically based on the relative location of the originating request.
- Applications can span multiple monitors. You can easily drag the HMI content from one monitor to another.
To design applications for the multi-monitor deployment, in the SE client configuration file, enable the multi-monitor option and configure each monitor accordingly.
Provide Feedback