Edit general HMI server properties
Use the HMI server
Properties
dialog box to edit the general properties.To edit general HMI server properties:
- InFactoryTalk View Studio, in the Explorer window, right-click the HMI server icon and selectProperties.
- In the HMI serverPropertiesdialog box, in theGeneraltab, edit an field if needed.
- ClickApplyto save the changes and keep the dialog box open, or clickOKto save the changes and close the dialog box.
Provide Feedback