Set up OLE verb animation
Use the OLE Verb option on the Animation menu to animate an OLE object using an OLE verb. To do this you set up an expression, which when it evaluates to true, activates the specified OLE verb. The verbs available depend upon the object that is selected. This command is only available for OLE objects.
To set up OLE verb animation:
- In theGraphicseditor, right-click theOLEobject and then clickAnimation>OLE Verb.
- In theAnimationdialog box, in theOLE Verbtab, in theExpressionfield, type a tag name or an expression that will evaluate to True or False at runtime. Non-zero values indicate true, while zero indicates false.You can also clickTagto browse for a tag, or clickExpressionto open theExpressionEditorto create one.
- Specify a security code for the object if you plan to restrict who can activate the verb.
Provide Feedback