Property Panel - Properties tab

How do I open the Properties tab of the Property Panel
  1. In the
    Graphics
    editor, on a display, right-click the object and then select
    Property Panel
    .
  2. In the
    Property Panel
    , click the
    Properties
    tab.
The
Properties
tab of the
Property Panel
displays all the properties that are not hidden, of the graphic object that is currently selected. If more than one object is selected in the display, their combined properties are shown and
Multiple Selection
is displayed below the title bar instead of an object's name.
There are two columns in the
Properties
tab: one for a property's name and one for its value. A vertical scroll bar on the right lets you scroll through the properties if the list is too long to be displayed all at once.
The field below the columns displays the name of the property that is currently highlighted, along with its type and description. When a description is too long to fit in the box, use scroll bar on the right side to display it. A splitter bar between the grid and description box lets you resize these two areas relative to each other.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal