Using the Connections tab
In the
Connections
tab of the property panel you can assign a tag to some properties, and a tag or expression to others, for certain graphic objects. You can also remove the tag or expression after assignment.At runtime, changes in the value of the tag or expression will be reflected in changes to the property. For example, if the property is used in the animation for an object, changes to the value of the tag or expression will be reflected in the object's appearance or behavior at runtime.
TIP:
The Graphics editor's
Undo
and Redo
options operate on changes made in the Connections
tab, and take effect whether or not the Property Panel
is displayed or the object is selected.The
Connections
tab is also available in the Properties
dialog box for those graphic objects that can use connections.Provide Feedback