Connections tab

How do I open the Connections tab?
In the
Graphics
editor, do one of the following:
  • On a display, click an object. In the
    Property Panel
    , click the
    Connections
    tab.
  • In the
    Properties
    dialog box of graphic objects that can use connections, click the
    Connections
    tab.
The
Connections
tab shows all the available properties of the selected object that can be connected to a tag or expression. It does not show non-bindable, read-only properties, or the extended properties provided by the Graphics editor. If more than one object is selected on the display, nothing is shown in the
Connections
tab.
You can assign a tag or specify an expression to the property in the grid. The box below the grid shows the name, type and description of the property that is currently selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal