Create a signature button
The Signature Button is an ActiveX object. You can put it on a display to control the actions that can be performed by the operator at runtime.
To create a signature button:
- InFactoryTalk View Studio, in the Graphics editor, open the display you are going to put a signature button on.
- From the menu, selectObjects>Advanced>Signature, or click theSignatureicon in the toolbox.
- On the display, drag the mouse to draw a box the approximate size the signature button is to be.
- In theFactoryTalk View SE Signature Button Propertiesdialog box tabs, set up how the button will operate and what it will look like at runtime. For details about instructions, clickHelpon each tab.
TIP:
Change the font style and color using the Font property on the Properties tab of the Property Panel.
Set other properties for the button here, such as ForeColor and BackColor.
Provide Feedback