Set up runtime behavior for a signature button

The authentication dialog box is displayed at runtime when the operator clicks the signature button. In the Signature tab you set up how the authentication dialog box will behave.
To set up runtime behavior for a signature button:
  1. In the
    Signature
    tab, in the
    Operation
    list, select an operation that the button will perform when the signature is verified.
    You may need to specify additional information depending on the operation selected. For details, see the
    Operation
    section below.
  2. Type a window title and description of the operation.
  3. Specify the domain for the operator and approver who will perform the authentication, and which levels of authentication will be required. You can choose groups for both the operator and approver rather than individuals, if necessary.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal