Signature Button Properties - General tab
In the
General
tab you type the caption that will be displayed on the button at runtime.Button Caption
Type the text that is to be displayed on the face of the signature button at runtime.
Provide Feedback