Create a navigation button
Use the
Navigation
option under Object
menu to create a navigation button.To create a navigation button:
- In theGraphicseditor, selectObjects>Push Button>Navigation,or click the navigation button icon in theObjectstoolbox.
- Drag the mouse to position and draw a shape the general size and location you intend the button to be. When you release the mouse button, theNavigation Button Propertiesdialog is displayed.
- In theNavigation Button Propertiesdialog box, configure the properties if needed.
Provide Feedback