Set up the active appearance of a navigation button

Use the Active Appearance tab to set up the active appearance.
To set up the active appearance for a navigation button:
  1. In a display, double-click the object to open the Navigation Button Properties dialog box.
  2. Click the
    Active Appearance
    tab.
  3. Specify these properties:
    • General appearance
    • Caption, if any
    • Image settings, if any
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal