Set up general properties for a navigation button

Use the
General
tab to set up general properties for a navigation button. After you set up the options in the General tab, click the
Active Appearance
and
Inactive Appearance
tabs to specify how the button looks at runtime.
IMPORTANT:
Make sure you select the
Track Screen for Navigation
check box for the displays you want to navigate between.
The option is in the
Display Settings
dialog box. By default, the check box is selected, and the display is added to the navigation history when it is opened.
To set up general properties for a navigation button:
  1. In the
    Navigation Button Properties
    dialog box, select the
    General
    tab.
  2. In the
    General
    tab, specify these properties:
    • General appearance under
      Appearance
      .
    • Type of action the button initiates under
      Action
      .
    • Touch-insensitive margins under
      Touch margins
      .
    • Audio (whether the button beeps at runtime) under
      Other
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal