Set up the inactive appearance of a navigation button
Use the
Inactive Appearance
tab to set up the inactive appearance of a navigation button.By default, the
Same as Active Appearance
check box is selected and the inactive appearance settings are set the same as the active appearance settings. If your system does not require a different inactive appearance from the active appearance, you do not have to specify additional settings in this tab.To set up the inactive appearance of a navigation button:
- In the Navigation Button Properties dialog box, select theInactive Appearancetab.
- In theInactive Appearancetab, clear theSame as Active Appearancecheck box.
- Specify these properties as you want:
- General appearance
- Caption
- Image settings
Provide Feedback