Create a maintained button
Use the maintained push button object to create a button that toggles between two values. This type of button is useful for changing a setting within a machine or process, but not for starting the machine or process.
A maintained push button sends one value to the data source the first time it is pressed, and a second value the next time it is pressed and released.
IMPORTANT:
Do not use push buttons for emergency stops. Emergency stop buttons must be hard-wired.
To create a maintained push button:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Push Button>Maintained, or click the maintained push button icon in the toolbox.
- Drag the mouse to position and draw a rectangle the general size and location you intend the button to be.
- In theMaintained Push Button Propertiesdialog box, specify how the button looks, how to change states, and its tags.
Provide Feedback